2022-12-12 06:40 AM
Hi ST Team,
i use the SMBJ30A/CA but how much current will be flow if a DC voltage of 40 volt is applied? It must be larger than IBR = 1 mA given in the datasheet. However, there isn't any info for DC operation if a DC voltage above VBR but below VCL is constant applied. Without this info it is not possible to calculate the power dissipation in the whole path.
Thanks