2005-06-01 03:59 AM
2011-05-17 03:07 AM
Hello!
what is the difference whit the I/O port of MCU P1,P3,P4 and the I/O port OF PSD PortA, PortB,PortC, PortD2011-05-17 03:07 AM
There are pretty significant differences. The MCU ports (P1, P3, and P4) basically have the same electrical characteristics as the Intel 8032AH MCU. This means that they're TTL-compatible and not CMOS technology. The PSD ports ARE CMOS ports which means that have much higher Voh and lower Vol. Additionally, they're capable of sinking / sourcing far more current than the MCU ports. Finally, the PSD ports can interact with the programmable logic to automatically serve different functions (chip selects, etc.).