cancel
Showing results for 
Search instead for 
Did you mean: 

Pin layout of DB501 & DB502 adapters from ST92F150-EMU2 emulator

Posted on October 28, 2002 at 17:18

Pin layout of DB501 & DB502 adapters from ST92F150-EMU2 emulator

2 REPLIES 2
Posted on May 17, 2011 at 11:32

I am looking for the pin layout of the following items from the ST92F150-EMU2 HDS2V2 emulator :

- the TQFP100 side of the TQFP100 (14x14) rigid adapter (DB502)

and

- TQFP100 (14x14) flat cable adapter (DB501B)

I did not find it in the ST92F150-EMU2 emulator user manual

Anyone ?

Jojo

johanpauvert1
Associate II
Posted on May 17, 2011 at 11:32

Since I did not find the layout in any ST9F150 document,

I tested the DB501B myself and came up with the enclosed layout (see db5pdf).

I also tested the DB502 this morning and it looks like this is the same layout as the DB501 one.

Breizh