cancel
Showing results for 
Search instead for 
Did you mean: 

M24M02-DRMN6TP Please share the Body Marking

Mylu Srinivasulu
Associate

Dear Team,

Can you please help us for the Body marking clarification for the MPN#M24M02-DRMN6TP

We have received the part with the body marking : 24M02RD

 

 

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @Mylu Srinivasulu, to the community!

I can confirm that the M24M02-DRMN6TP has the marking 24M02RD. The letter K in the lower right corner also corresponds to the current marking.

The three-digit number sequence in front of it (322 in your case) indicates the production date: last digit of the year (3) and two digits of the calendar week (22). Since the M2 was only launched in 2010, the digit of the year can (currently) only be interpreted as 2013 or 2023.

If the problem is solved, please click Accept as Solution. This will help other users find that answer faster.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.