2023-08-17 02:56 AM
Dear Team,
Can you please help us for the Body marking clarification for the MPN#M24M02-DRMN6TP
We have received the part with the body marking : 24M02RD
2023-08-17 11:29 PM - edited 2023-08-17 11:30 PM
Welcome @Mylu Srinivasulu, to the community!
I can confirm that the M24M02-DRMN6TP has the marking 24M02RD. The letter K in the lower right corner also corresponds to the current marking.
The three-digit number sequence in front of it (322 in your case) indicates the production date: last digit of the year (3) and two digits of the calendar week (22). Since the M2 was only launched in 2010, the digit of the year can (currently) only be interpreted as 2013 or 2023.
If the problem is solved, please click Accept as Solution. This will help other users find that answer faster.
Regards
/Peter