2005-12-01 08:20 PM
2005-11-30 12:11 AM
Hello all,
I have to implement a MENU screen including a few sub menu's on a 230x240 pixel LCD display. Selecting sub-menu's is done through digital inputs(buttons). I can poll these inputs or generate an interrupt to detect an active input. I can write everything on the display I want to. So I can build the individial menu screens. My problem is how do I implement a software structure to write the different menu's and sub-menu's to the screen. Does someone have an idea or an example? Thanks, Jimmey2005-11-30 05:46 AM
Hi Iamanil,
I am working with a 240x240 pixel display black/white. My interface is an indirect parrallel bus no SPI bus. My controller is the Epson S1D13700. Sorry but I can not help you. Regards, Jimmey