Posted on May 28, 2009 at 12:10Dear all, When I have only one node on the CAN bus and this node is start sending data it will never stop transmitting. Of course this is because there is no other node to answer/reply. However in all the ST library/ex...
Posted on February 28, 2007 at 05:41hi and thanks, I checked already but there is no wachtdog initialisation in the startup code. The strange thing is that I programmed the bigger STR710 before and I never had this problem before. I stopped the prog...
Posted on February 28, 2007 at 04:57Hi all, I am using Uvision3 from Keil to develop software for the STR715 MCU. However when debugging from SRAM I am not able to disable the watchdog. When(during debugging) the program is loaded in the SRAM the pr...
Posted on December 27, 2006 at 11:09Hi Sander, This is how I solved the problem. I am using 3 analog ports to read in one signal now. On the firts I put the signal that want to read in(signal with the information). On the second input I putted a (LT...
Posted on November 20, 2006 at 10:06Hi all, I am using the ADC of the STR710 MCU at it's maximum resolution. Now I have some trouble with reading in analog signals with mV accuraty. If I put 0,000V on the input the ADC outputs(after avaraging 32 sam...