cancel
Showing results for 
Search instead for 
Did you mean: 

I didn't found ST10R167 JTAG/Programming port. Can any know this please post.

GPand.3
Associate II
 
8 REPLIES 8
Peter BENSCH
ST Employee

Welcome, @GPand.3​, to the community!

I moved the thread to Discontinued Products, since the ST10R167 has been discontinued a long time ago.

About your question: the ST10R167 doesn't have a JTAG port, so you can't plug a JTAG debugger into it.

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Yes it's discontinued, but is' for our existing board, where is the programming PIN's.

The ST10R167 also has no programmable memory, so there is no point in connecting a programmer.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
GPand.3
Associate II

Yes memory, so If we connect an external Flash Memory then?

Regards

Gangadhar

GPand.3
Associate II

Yes no programmable memory, so If we connect an external Flash Memory then?

Well, you wrote that this is an existing board, so there must already be memory?

External flash is already a challenge because you will hardly find any flash with 5V supply voltage. But if you connect one, you'll either have to program it externally or use a program you wrote yourself for the MCU via one of the communication ports.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

So guessing all the engineers responsible for this product work some place else now? That's unfortunate, will any of them contract support?

D​id you buy flash parts preprogrammed? Program parts you provided to the PCBA? Some kind of header or bed-of-nails fixture to program in production?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
lsun.1
Associate II

st10r167 has 32kB internal ROM
_legacyfs_online_stmicro_images_0693W00000bjE3RQAU.pngIt can be programed by TXD and RXD, st10 flasher tools


_legacyfs_online_stmicro_images_0693W00000bjE3vQAE.png