2006-01-04 02:53 AM
How to download my .d79 file not using IAR IDE
2005-11-13 10:06 PM
I have compiled my project into .d79 and .sim files, and i have a jlink simulator to connect to jtag interface, but i don't want to download my program in IAR IDE with openning my project everytime, do you have any good ways to download my program through other ways?
2005-11-13 10:23 PM
I got my answer, thank you!
2005-12-22 10:40 AM
I have the same question. Where did you find the answer?
Thanks, Doug2006-01-04 02:53 AM
Hi Doug,
I got an answer in another thread, ''PLS , SEGGER and Raisonance provides Programmers for STR7. '' I would however recommend you try to burn a raw binary file into the flash, instead of the .sim file from the debug process of IAR. (That is true only if you are targeting production, 'cuz that'll remove all debug info...) Hope this helps a little... Regards, Jp