Posted on January 11, 2006 at 17:59I'm wondering the same thing. From my experimentation, the SS pin must be pulled up, rendering the pin useless when using the SPI as the master. There must be something I'm not understanding.
Posted on December 19, 2005 at 18:23There are a few questions I have about the ADC conversion offset thread: 1) Is Frank Anderson correct about the comment in the example calibration code that the 1830 mV should have been 2500 mV? 2) Why did ST make...