cancel
Showing results for 
Search instead for 
Did you mean: 

how to access internal eeprom str750

starfish844
Associate II
Posted on October 13, 2009 at 18:45

how to access internal eeprom str750

2 REPLIES 2
starfish844
Associate II
Posted on September 17, 2009 at 04:24

Hi all,

i am using keil mcbstr750 evaluation board. I have a problem. I create a LCD menu showing various datas which is get from ADC. In addition, i defined some alarms (i.e ''Power High'' ). When the alarm occurs, a LED is turn on. At the same time, i want to write this alarm internal eeprom(16kb). Whwnever i want i read this.For example, In a ''Power High'' alarm condition, in ''Event Log'' menu i have prepeared, i want to see ''Power High:20-09-2009''.

How can i do that?

Thank you for your help.

Best Regards.

tomas23
Associate II
Posted on October 13, 2009 at 18:45

There is no EEPROM inside STR750 or on the Keil board, AFAIK. Either place some EEPROM externally on the I2C bus (and manage to talk to it via I2C) on the soldering area of that board, or check the EEPROM emulation, there exists AN on this topic in some of ARM family.

You'll need the Flash programming manual for STR7xx MCUs, too.