cancel
Showing results for 
Search instead for 
Did you mean: 

Error opening visual programmer

sanjayakp
Associate II
Posted on July 09, 2009 at 11:21

Error opening visual programmer

6 REPLIES 6
sanjayakp
Associate II
Posted on April 30, 2009 at 20:48

I installed ST toolset new program in windows 2000.

When I tried to open the st visual programmer, I recieved a message window saying ''Cannot load JICC_API Dll'' even before vis. programmer window appears.

And Then brings up the configuration setting. I choose my micro and say OK, but it brings up another window saying ''choose a valid configuration''.

Need your help.

Thanks

sanjaya

________________

Attachments :

1.bmp : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0GG&d=%2Fa%2F0X0000000bWG%2F4uFRfIeyTmv2Fhi8VOfQlrXN6RHn3UOyqtFkgqLjqv4&asPdf=false
wolfgang2399
Associate II
Posted on May 05, 2009 at 12:32

Hi Sanjaya,

Exactly the same happens to me - with win2000 and the new ST toolset (pack17).

Because I'm only using the programming mode (STVP), I've re-installed the STtoolset-pack15 as workaround and all the features work fine.

Nevertheless, I'm curious when STM will fix this bug...

Regards,

WoRo

sanjayakp
Associate II
Posted on May 06, 2009 at 20:23

Thanks a lot for the info.

Can you help sending me the link for stttoolset pack 15.

Thanks in advance.

sanjaya

wolfgang2399
Associate II
Posted on May 07, 2009 at 11:40

Hi Sanjaya,

there are no known links to older versions. I tried to upload the whole file and to append it here, but I failed. :(

Most probably it is the best way you ask your local distributor.

Nevertheless I think you would really promote this forum when you make our highly devoteded moderators discharge their duties ...

Greetings,

WoRo

wolfgang2399
Associate II
Posted on May 07, 2009 at 12:21

...succeeded in packing the file to a .zip file and attaching it here.

You only have to extract the enclosed file. :)

Regards,

WoRo

________________

Attachments :

st7toolset_Pack15.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hzne&d=%2Fa%2F0X0000000bWH%2FOxuivRD88T_5Rnw4fnKGOFph5wW6lSxa8Oodkps5oBY&asPdf=false
wolfgang2399
Associate II
Posted on July 09, 2009 at 11:21

Hi to all Users (as well as to the Moderators :-o)

I became aware of that my attachement from 2009-05-07 could not work because the file has been corrupted - sorry.

I'll try again to attach a .zip file of pack Hope it works now.

BTW: Even in sttoolset Pack 18 the experts of STM did not fix the bug...

WoRo

________________

Attachments :

st7toolset_pack15.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0G6&d=%2Fa%2F0X0000000bWF%2FEF28PEedOH1DQ4NCBEYxy.I5lfpXJa6NYxG05v8ImGU&asPdf=false