2023-10-25 07:00 AM
Hello, folks.
I'm using the STHV1600 (specifically its evaluation kit board, the STEVAL-IME014V1B) for my thesis on sonothrombolysis. For this ultrasound application, I need multiple time delay configurations for the pulses (approximately 400). The GUI provided with the evaluation kit only allows me to set one configuration in the IC. Is there another method to configure the memory and time delay schema without the limitations of the GUI?
2024-02-14 04:15 AM
Hi JianVeras,
I am writing to see if you managed to progress on answering this question? I am facing the same issue of generating multiple delay profiles. In case it is not possible through the GUI software, my second idea was to program the Nucleo with the required patterns and timing functions to control the STHV1600 without the GUI, but I am not entirely sure whether that is the best option.
Any advice is highly appreciated.
Regards,
Bartas