2024-11-25 5:06 AM - edited 2024-11-25 5:07 AM
Hello everyone,
I get an error when booting Linux + initramfs
The versions of the main components are:
| Component | Version |
| tf-a-stm32mp | v2.6-stm32mp-r2.2 |
| optee-os-stm32mp | v3.16.0-stm32mp-r2.2 |
| u-boot-stm32mp | v2021.10-stm32mp-r2.2 |
| linux-stm32mp | v5.15.145-stm32mp-r2.2 |
bootcmd:
setenv boot_device mmc;
setenv boot_instance 0;
setenv boot_partition 5;
setenv fit_addr C2000000;
mmc partactive ${boot_instance};
mmc partconf ${boot_device} 1 1 0;
load ${boot_device} ${boot_instance}:${boot_partition} ${fit_addr} fitImage-foo-image-initramfs;
setenv bootargs console=ttySTM0,115200 FIT_IMAGE_PART=${boot_partition} debug loglevel=8;
bootm ${fit_addr};
error:
[ 2.588644] rootfs image is not initramfs (write error); looks like an initrd
[ 2.588766] /initrd.image: incomplete write (-28 != 32769317)
[ 2.753422] Freeing initrd memory: 32004K
From my research I found that:
-28: ENOSPCwhich means No space left on device.
If I add:
setenv initrd_high 0xFFFFFFFF
The error does not occur anymore. This is probably because the ramdisk is loaded directly from flash memory and not copied to RAM beforehand (see https://docs.u-boot.org/en/v2022.10/usage/environment.html)
The fitImage loading information states the following:
## Loading kernel from FIT Image at c2000000 ...
Using 'conf-stm32mp151c-foo.dtb' configuration
Trying 'kernel-1' kernel subimage
Description: Linux kernel
Created: 2023-12-23 9:42:00 UTC
Type: Kernel Image
Compression: uncompressed
Data Start: 0xc2000120
Data Size: 7437600 Bytes = 7.1 MiB
Architecture: ARM
OS: Linux
Load Address: 0xc0800000
Entry Point: 0xc0800000
Hash algo: sha256
Hash value: bf3e491301d2dc9fe63bf119ce4704a147f3dce0ca1168110ba7dd5b29e4cf63
Verifying Hash Integrity ... sha256+ OK
## Loading ramdisk from FIT Image at c2000000 ...
Using 'conf-stm32mp151c-foo.dtb' configuration
Trying 'ramdisk-1' ramdisk subimage
Description: foo-image-initramfs
Created: 2023-12-23 9:42:00 UTC
Type: RAMDisk Image
Compression: uncompressed
Data Start: 0xc2724e88
Data Size: 32769317 Bytes = 31.3 MiB
Architecture: ARM
OS: Linux
Load Address: unavailable
Entry Point: unavailable
Hash algo: sha256
Hash value: 47c1724633530ff00903486d1bf7d334fa46c55ff7afedcb96b403c74c8c629f
Verifying Hash Integrity ... sha256+ OK
## Loading fdt from FIT Image at c2000000 ...
Bootstage space exhasuted
Bootstage space exhasuted
Using 'conf-stm32mp151c-foo.dtb' configuration
Trying 'fdt-stm32mp151c-foo.dtb' fdt subimage
Description: Flattened Device Tree blob
Created: 2023-12-23 9:42:00 UTC
Type: Flat Device Tree
Compression: uncompressed
Data Start: 0xc2717f54
Data Size: 52840 Bytes = 51.6 KiB
Architecture: ARM
Hash algo: sha256
Hash value: 1744a9700ebbe4faa2f35112ff30749cab8d769a205d082a970c65e72303f243
Verifying Hash Integrity ... sha256+ OK
Bootstage space exhasuted
Bootstage space exhasuted
Bootstage space exhasuted
Bootstage space exhasuted
Bootstage space exhasuted
Booting using the fdt blob at 0xc2717f54
Loading Kernel Image
Bootstage space exhasuted
Bootstage space exhasuted
Loading Ramdisk to c9fbb000, end cbefb525 ... OK
Loading Device Tree to c9fab000, end c9fbae67 ... OK
Bootstage space exhasuted
Bootstage space exhasuted
Starting kernel ...
The ramdisk is successfully loaded into memory. But later on it can't be loaded into memory by the kernel?
The position c9fbb000 - cbefb525 is exactly the size of the initramfs 1F40525 = 32769317 bytes.
Compression of the initramfs
Has it something to do with the compression? Because the initramfs is in the format "cpio.gz" which means it is compressed with gzip. In the .its file (which is generated by yocto kernel-fitimage class) the compression is set to "none". If u-boot only allocates memory for the compressed initramfs and the kernel later on decompresses it and tries to load it into the same memory position it does not fit anymore maybe?
Any information on what is actually happening while this fitImage is booting would be appreciated.