2007-03-27 11:15 PM
2011-05-17 12:40 AM
Hi,
I would like to transfer data from an external memory and internal memory from/to a single external memory location in a FPGA. These data contain modified camera data in CIF format and compressed encrypted video data to a optical data link. However, I would like to let the FPGA start a burst or single word transfer from/to external PSRAM location into/from FPGA adress space. There are 2 possible external DMA request pins. How do they work? level/edge triggered? falling/rising/low/high? What are the timings? Is there a spec anywhere? What is the max. speed at 96 MHz? etc. Please help me! regards, Gerhard.