cancel
Showing results for 
Search instead for 
Did you mean: 

Enable performance monitor

David Dieckow
Associate II
Posted on December 05, 2017 at 14:04

Hi,

I'm trying to enable performance monitor on SPC58x series without luck so far. I tried the following:

        e_lis       %r3, 0x8000

        e_or2i      %r3, 0x0000

        mtpmr       400, %r3 # freeze all global counters

        e_lis       %r3, 0x27

        e_or2i      %r3, 0x0000 #event 39

        mtpmr       144, %r3 #set up pipeline stall event in counter 0

        e_lis       %r3, 0x39

        e_or2i      %r3, 0x0000 #event 57

        mtpmr       145, %r3 #set up data cache line fills event in counter 1

        e_lis       %r3, 0x0

        e_or2i      %r3, 0x0

        mtpmr       400, %r3 # un-freeze all global counters

But the counter register (PMCx) do not increase at all. What am I missing?

Thank's, David

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
Erwan YVIN
ST Employee
Posted on December 06, 2017 at 11:10

Hello David ,

There is a useful document from NXP Side.

it is the same core. There are some slides how to setup the PMR.

https://community.nxp.com/docs/DOC-105754

 

       Best regards

               Erwan

David Dieckow
Associate II
Posted on December 06, 2017 at 11:27

Hi Ewan,

thank's that might help, I will try. (Actually this document is from Freescale, STM does not provide much information on how to enable and use performance monitors, the datasheet is not very helpful).

I also used

https://www.google.de/url?sa=t&rct=j&q=&esrc=s&source=web&cd=1&cad=rja&uact=8&ved=0ahUKEwi0r97mlfXXAhVEPFAKHbEcB3IQFggqMAA&url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN4341.pdf&usg=AOvVaw2TKmrmcTThhV7SKlHvZ2lI

document from NXP that explains how performance monitor can be used, thats were I got the sample code from. The register structure is a little bit different between NXP and STM perfomance monitor but I already adapted this to STM register structure. I also read somethimg about SPU but don't know what I should to with it to enable the performance monitor.

Regards,

David

Posted on December 07, 2017 at 09:23

Hello David ,

In Autosar part and SOC functional Valid part, they do not use PMR.

I think that in Autosar part, they use SPU chapter Sequence Processing Unit (SPU)

I am asking an application note about SPU.

                Best regards

                                      Erwan

Posted on December 07, 2017 at 09:38

Hi Erwan,

I don't use Autosar but bare-metal OS. I don't understand how PMR and SPU do work together or are they independent?

Regards,

David

Posted on December 11, 2017 at 08:12

Dear Erwan,

sorry, but the document does not really help. Still the performance monitor is not counting.

Do you have any other suggestions I might look into?

Thank's and regards,

David

Posted on December 11, 2017 at 10:09

Hello David ,

After investigation cf Chap 13 Debug and Trace and Chap 64 RM0407

Soc Functional valid team are using cmm script (Trace32) to enable the SPU

(cf SPU_SE Table 1445)

      Best regards

              Erwan

Posted on December 11, 2017 at 10:25

Dear Erwan,

I cannot find RM0407 can you provide a link?

Also I don't use Trace32 for debugging but UDE STK (latest version 4.8.6). Nervertheless, can you provide the CMM-Script or tell me how I can do the same with UDE STK (or at least how to activate it by code).

So my assumption is correct that SPU needs to be configured to activate performance monitor?

Regards,

David

Posted on December 11, 2017 at 10:35

Hello David ,

could you give me your MCU used ?

because the RM should be given by an other way. (by marketing way or field application engineer)

              Best regards

                               Erwan