2017-12-05 5:04 AM
Hi,
I'm trying to enable performance monitor on SPC58x series without luck so far. I tried the following:
e_lis %r3, 0x8000
e_or2i %r3, 0x0000 mtpmr 400, %r3 # freeze all global counterse_lis %r3, 0x27
e_or2i %r3, 0x0000 #event 39 mtpmr 144, %r3 #set up pipeline stall event in counter 0e_lis %r3, 0x39
e_or2i %r3, 0x0000 #event 57 mtpmr 145, %r3 #set up data cache line fills event in counter 1e_lis %r3, 0x0
e_or2i %r3, 0x0 mtpmr 400, %r3 # un-freeze all global countersBut the counter register (PMCx) do not increase at all. What am I missing?
Thank's, David
2017-12-06 2:10 AM
Hello David ,
There is a useful document from NXP Side.
it is the same core. There are some slides how to setup the PMR.
https://community.nxp.com/docs/DOC-105754
Best regards
Erwan
2017-12-06 2:27 AM
Hi Ewan,
thank's that might help, I will try. (Actually this document is from Freescale, STM does not provide much information on how to enable and use performance monitors, the datasheet is not very helpful).
I also used
document from NXP that explains how performance monitor can be used, thats were I got the sample code from. The register structure is a little bit different between NXP and STM perfomance monitor but I already adapted this to STM register structure. I also read somethimg about SPU but don't know what I should to with it to enable the performance monitor.Regards,
David
2017-12-07 1:23 AM
Hello David ,
In Autosar part and SOC functional Valid part, they do not use PMR.
I think that in Autosar part, they use SPU chapter Sequence Processing Unit (SPU)
I am asking an application note about SPU.
Best regards
Erwan
2017-12-07 1:38 AM
Hi Erwan,
I don't use Autosar but bare-metal OS. I don't understand how PMR and SPU do work together or are they independent?
Regards,
David
2017-12-11 12:12 AM
Dear Erwan,
sorry, but the document does not really help. Still the performance monitor is not counting.
Do you have any other suggestions I might look into?
Thank's and regards,
David
2017-12-11 2:09 AM
Hello David ,
After investigation cf Chap 13 Debug and Trace and Chap 64 RM0407
Soc Functional valid team are using cmm script (Trace32) to enable the SPU
(cf SPU_SE Table 1445)
Best regards
Erwan
2017-12-11 2:25 AM
Dear Erwan,
I cannot find RM0407 can you provide a link?
Also I don't use Trace32 for debugging but UDE STK (latest version 4.8.6). Nervertheless, can you provide the CMM-Script or tell me how I can do the same with UDE STK (or at least how to activate it by code).
So my assumption is correct that SPU needs to be configured to activate performance monitor?
Regards,
David
2017-12-11 2:35 AM
Hello David ,
could you give me your MCU used ?
because the RM should be given by an other way. (by marketing way or field application engineer)
Best regards
Erwan