cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5 update can not apply GTM patches

Larsa
Associate II

We have just ran the update for SPC5 and on regenerating the application we get this message. What can we do to solve that?

/Larsa

0693W00000DnwBMQAZ.jpg

1 ACCEPTED SOLUTION

Accepted Solutions
ECAST.1
Associate II

Hello,

the customization (in driver source files) are memorized in a project file "patch.xml" (available in the root directory of the project).

Every time that the User re-generate the code, the customization are applied to the source files.

This message is reported when the patches are no more necessary (patch code is already present in the source file) or when totally not aligned with the source file.

If, it is in the second case, please apply the patch manually, ignoring the SPC5Studio message.

BR,

Emanuele

View solution in original post

2 REPLIES 2
ECAST.1
Associate II

Hello,

the customization (in driver source files) are memorized in a project file "patch.xml" (available in the root directory of the project).

Every time that the User re-generate the code, the customization are applied to the source files.

This message is reported when the patches are no more necessary (patch code is already present in the source file) or when totally not aligned with the source file.

If, it is in the second case, please apply the patch manually, ignoring the SPC5Studio message.

BR,

Emanuele

Larsa
Associate II

That makes sense, thanks Emanuele!