Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! ADC library header

Hi, i want to ask regarding the sensor library. As i new to SPC5Studio, i want to connect the displacement sensor. So , do i need to declare the sensor library as a header or just simply can use the ADC header library?

Angle by Associate II
  • 1321 Views
  • 3 replies
  • 0 kudos

Resolved! irqIsrEnable Debug Crash

Hi,i have spc560p50l5 if i enable irqIsrEnable(); in debug it crash. (no codes execuded after).If i comment //irqIsrEnable(); debug works, but osal not starts.In assembly code of swirq_enable there are a lot OF_SE_ILLEGAL0x400001E8 00 00    SE_ILLEGA...

eirq interrupt

Hi, can anyone share to me the code for push button that using eirq interrupt? I do see on the example and also successfully build with no error. But when i debug and try to my hardware, nothing happened. LED do not blink when i click on push button

Angle by Associate II
  • 759 Views
  • 1 replies
  • 0 kudos

1. to make non cache area in the SPC58NH, making memory attribute to Cache-inhibit is right? 2. what is difference between data descriptors and shared descriptors? 3.The SPC58NH does not support write-through attribute for cache? if can how?

1. to make non cache area in the SPC58NH, making memory attribute to Cache-inhibit is right?2. what is difference between data descriptors and shared descriptors?3.The SPC58NH does not support write-through attribute for cache? if can how? 

Calculating faster

Hello,​ I'm working with spc560p and I want to calculate my code my code more faster as usual. I Impelement PIT DRIVER too for other use of my mcu. Is there any method to calculating faster?​Thanks for your attention

DNewm.1 by Associate III
  • 1029 Views
  • 1 replies
  • 0 kudos

Sensor Driver

Hi, can i know which driver use for displacement sensor? and also can i know which one is the example code for the sensor so that i can refer

Angle by Associate II
  • 552 Views
  • 0 replies
  • 0 kudos