Hello,I've used your code in a SPC5Studio project for Bernina MCU, and the correct value of Duty and Period are triggered. Come back to the original issue...The TOM0_4 starts with settings period = 10000 and duty= 5000The TOM0_3 starts with settings ...
Hello,Errata sheet are available on web-site:https://www.st.com/en/automotive-microcontrollers/spc572l64f2.html#documentationSome work around in the DPLL area, one of them could be useful for your issue.Regards,Emanuele
Hello,If the ATOM timed pulse are ATOM configured in SOMC mode the feature about RDADDR0 / RDADDR1 could help you... I don't knowOr the PWM signal to control the injection could be configure in immediate mode(SOMI), in this case the MCS assembler cod...
Hello,the customization (in driver source files) are memorized in a project file "patch.xml" (available in the root directory of the project).Every time that the User re-generate the code, the customization are applied to the source files.This messag...
Hello Lars,Please see the document at link: https://www.st.com/resource/en/reference_manual/rm0361-generic-timer-module-specification-revision-1551-stmicroelectronics.pdfThis is the reference manual for GTM on SPC572L ST MCU.The number of MCS instanc...