2023-04-05 07:14 PM - edited 2023-11-20 08:51 AM
I have a L9963E BMS development board, I have tried connecting to SPC5 UDESTK Debugger, the debugger is not getting connected (UDE STK Debugger) to the controller I have connected the power adapter and USB mini connector as well, I am using UDESTK Staterkit 2021 version from pls.
The error indicates No Target Supply or JTAG Cable Connection or Target Configuration
Target
Configuration I have selected from the provided list
Power to the board is proper I have connected the adapter and to rule out if it is taking power from USB of Serial cable, I have connected the serial cable i.e., the FTDI cable as well
To
Confirm the power to the board is fine, I have ran the default firmware which
is shipped along with the board, it is getting connected to the
L9963_evaluation_GUI program and serial communication is OK.
how can we connect the debugger, any settings needed in the development board to be done or any jumper settings need to be changed?
Also
Is there a facility to connect the board via STLINK?
2023-04-06 11:07 PM
The L9963E BMS board is a battery management system board used for managing battery cells in electric vehicles. The UDESTK connection is used for debugging and programming the board. If you are experiencing issues with the UDESTK connection, here are some troubleshooting steps you can try:
It's important to note that programming and debugging BMS boards can be complex and requires technical expertise. If you're not familiar with the process, it's recommended that you seek help from an experienced technician or engineer to avoid causing any damage to the board.
2023-04-13 09:26 AM
Thank you for your response. But as you mentioned for point 2
Verify the UDESTK settings: Check the UDESTK settings to ensure that the correct baud rate and other settings are selected for the programming tool
--> I could see the JTAG lines are directly connected to the Controller are there any specific setting or jumper settings need to be done?