cancel
Showing results for 
Search instead for 
Did you mean: 

UDE STK tool does not detect target client after new target configuration for SPC5746CBMKU6 board

shivani1
Associate

I want to flash and debug using SPC5-UDESTK 5.02.04 on to the board SPC5746CBMKU6. This controller configuration is not given in the tool. So I have created new configuration for this board. Now I have tried to connect to target board. But it is failing to establish connection. 

shivani1_0-1709885305550.png

Connection and power supply is good(Tool LED glows). May be problem with target configuration. 

Attaching failed report and new target configuration file(in .txt, as .cfg is not supported here). Kindly provide the target configuration file for SPC5746CBMKU6, if you have. Or suggest edits in current file. 

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Hello ,

The board SPC5746CBMKU6 is a processor coming from NXP side.

I recommend to check with them.

I do not known if there is PLS Ftdi in this board.

                   Best regards

                                Erwan

  

 

 

View solution in original post

1 REPLY 1
Erwan YVIN
ST Employee

Hello ,

The board SPC5746CBMKU6 is a processor coming from NXP side.

I recommend to check with them.

I do not known if there is PLS Ftdi in this board.

                   Best regards

                                Erwan