cancel
Showing results for 
Search instead for 
Did you mean: 

Can EVALSTDRIVE101 drive a BLAC motor?

Nicholas_minafra97
Associate

hello everyone, i'd like to know if i can use the EVALSTDRIVE101 add-on board driven by an stm32-nucleo to drive BLAC motors. Because the datasheet says that they are suitable for BLDC AND PMSM.

Otherwise there is some other board that allows driving  blac motors?

1 ACCEPTED SOLUTION

Accepted Solutions

STEVAL-IPM15B Can work with STM32 boards but it supports DC Motors not AC.

Best regards.

II

View solution in original post

3 REPLIES 3
Issamos
Lead II

Hello @Nicholas_minafra97 

As you can see in this description 

Screenshot_2023-09-05-16-31-41-51_40deb401b9ffe8e1df2f1cc5ba480b12.jpg

The EVALSTDRIVE101 is designed to drive three-phase brushless DC motors.

That's why it can't drive BLAC motors.

For AC motors driver, I suggest you to take a look at this .

Best regards.

II

Nicholas_minafra97
Associate

hello, @Issamos 

Can you tell me if STEVAL-IPM15B can be driven by a stm32-nucleo and if it can drive a BLAC motor ?

thank you.

 

STEVAL-IPM15B Can work with STM32 boards but it supports DC Motors not AC.

Best regards.

II