2018-10-17 06:05 PM
LIS2DH12, Zero-g level offset is 40mg at FS bit set to '00'.
When using the FS bit set to '11' and Normal resolution mode, what value is it?
40mg * 12 = 480mg ?
or
40mg * 48 = 1920mg?
Solved! Go to Solution.
2018-10-22 05:40 AM
ST doesn't specify this value.
But I would expect that if the zero-g level at FS=2g is typically 40mg, for FS=16g it could be 8-times higher.
2018-10-22 05:40 AM
ST doesn't specify this value.
But I would expect that if the zero-g level at FS=2g is typically 40mg, for FS=16g it could be 8-times higher.
2018-10-22 05:28 PM
Dear Miroslav BATEK,
Thank you for your reply.
But, I don't understand if zero-g level offset is affected by resolution mode(High resolution or Normal or Low-power).
Do not I have to worry about the resolution mode?
2018-10-24 12:50 AM
I don't think the resolution will have significant impact on the zero-g level.
2018-10-24 02:12 AM
Dear Miroslav BATEK.
Thank you!
Your answer was very helpful.