LIS2DH12, Zero-g level offset is 40mg at FS bit set to '00'.When using the FS bit set to '11' and Normal resolution mode, what value is it?40mg * 12 = 480mg ?or40mg * 48 = 1920mg?
Dear Miroslav BATEK,Thank you for your reply.But, I don't understand if zero-g level offset is affected by resolution mode(High resolution or Normal or Low-power).Do not I have to worry about the resolution mode?