2016-07-15 3:08 AM
Hello,
I just received the wesu board and I using it ''as it is'' with the related android app ST WeSU. What I'm facing looking at the cube on the app is that there is a very high drift of the cube itself. In details: if I move the board I see the cube moving coherently but when I put the board in a stable fixed position I see that cube take a very long time (up to 10/12 seconds, depending on the previous movements) to reach a fixed stable position. What could be the root cause? Thanks in advance Fabiano #wesu-drift2016-07-22 6:11 AM
Hello,
I have observed the same behavior.
It is a matter of fusion library. Lite version of fusion library is used in firmware of WeSu.
Best Regards,
Marian