To use ST BLE Sensor was not the right choose. It can be repaired using some programmer ST-Link, J-Link, Nucleo board, ... You have to flash again the binary file.
Hello, this is a strange behavior, because the default name should start with "AM1V" followed by version number. Are you using the binary from package or did you compile your own binary? Attached is binary from package 3.3.0 which is functional under...
Hi Cristian,algo_builder.c file is the part of source code which changes according to algorithm design.The rest of source code is placed inside directory specified in "Firmware Location" (see the picture).Inside sub directory "Projects" are placed co...
It is weird that you cannot write registry as administrator. Try to check again if you really start it as administrator. In Windows 10 you can use BLE communication in addition.
My first idea was that you have too new driver, but I checked it again and realize that there is no difference between newest driver and my current driver. I guess that driver change will not help. The new information is that you have Windows 7. My p...