cancel
Showing results for 
Search instead for 
Did you mean: 

Unicleo-GUI datalog's timestamp not working correctly

aesteban
Associate III

I'm working with a nucleo 401RE and a x-nucleo ISK 01A3 as hardware and algobuilder and unicleo-GUI as software. If I measure, for example, the rotation vector 9X throughout the day and save the output datalog using Unicleo-GUI, the timestamp shows that every hour and a quarter taking values, there is no data until hour and a half later, also the last timestamp shows that around 48h of data, so there is no data loss, just some weird cyclic jump error on the timestamp.

This error doesnt show up on Unicleo-GUI's user messages, just on the .csv timestamp generated.

How can i overcome this issue?

Any help is appreciated, thanks

1 ACCEPTED SOLUTION

Accepted Solutions
Miroslav BATEK
ST Employee

Hello @aesteban 

Yes, there is jump in timetsamp after approximately one hour and 15 minutes if you logging with Unicleo-GUI application. Would you please use MEMS Studio instead? The issue is not there.

View solution in original post

1 REPLY 1
Miroslav BATEK
ST Employee

Hello @aesteban 

Yes, there is jump in timetsamp after approximately one hour and 15 minutes if you logging with Unicleo-GUI application. Would you please use MEMS Studio instead? The issue is not there.