cancel
Showing results for 
Search instead for 
Did you mean: 

trying to interface with an HX711 load cell amp

GrantW
Associate II

The HX711 requires the MCU to send an exact number of clock pulses to capture a 24 bit value, then the clock signal must remain low until the HX711 indicates its ready to transmit again, using the data line. I tried to use a GPIO pin to generate the clock signal manually with pin_set and pin_reset calls, which works in that it creates a clock signal at the frequency of the APB, but the amplitude is only 100 mv. When I plug the clock signal into the HX711 the signal becomes low level noise. Here is the pin config:

  /*Configure GPIO pin : SCLK_Pin */
  GPIO_InitStruct.Pin = SCLK_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_PULLUP;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(SCLK_GPIO_Port, &GPIO_InitStruct);

and here is the clock gen code:

	// read 24 data bits
	for (i = 0; i < 24; i++) {
	    HAL_GPIO_WritePin (SCLK_GPIO_Port, SCLK_Pin, GPIO_PIN_SET);
	    buffer <<= 1;
	    HAL_GPIO_WritePin (SCLK_GPIO_Port, SCLK_Pin, GPIO_PIN_RESET);
	    buffer += HAL_GPIO_ReadPin (SDATA_GPIO_Port, SDATA_Pin);
	}

I should be getting a 3.3V clock signal. Any suggestions?

28 REPLIES 28
Uwe Bonnes
Principal III

Remember that SCK high longer than 50 us resets the chip. So block interrupts before you set SCK high and unblock after you have reset SCK.

HI BROS,

I finally did it.Thank you for your help.

It works properly.

CODE:

#include "main.h"

#include "stm32f4xx_hal.h"

void SystemClock_Config(void);

static void MX_GPIO_Init(void);

uint8_t value=0;

uint8_t i = 0;

int32_t adc_value = 0;

#define pause for(int n=0;n<100;n++){};

int main(void)

{

 HAL_Init();

 SystemClock_Config();

 MX_GPIO_Init();

 while (1)

 {

 while (HAL_GPIO_ReadPin(GPIOD, GPIO_PIN_15));

 for(i=0;i<25;i++)

 {

 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_SET);

 //pause

 adc_value <<= 1;

 if(HAL_GPIO_ReadPin(GPIOD, GPIO_PIN_15))adc_value++;

 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_RESET);

 //pause

 };

for (int i = 0; i < 128; i++) {

HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_SET);

HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_RESET);

}

//adc_value = adc_value ^ 0x800000;

  while(adc_value>=255)adc_value>>=8;

  value=adc_value;

  adc_value=0;

 }

 }

void SystemClock_Config(void)

{

 RCC_OscInitTypeDef RCC_OscInitStruct = {0};

 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage

 */

 __HAL_RCC_PWR_CLK_ENABLE();

 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the CPU, AHB and APB busses clocks

 */

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

 RCC_OscInitStruct.HSIState = RCC_HSI_ON;

 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;

 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

 RCC_OscInitStruct.PLL.PLLM = 8;

 RCC_OscInitStruct.PLL.PLLN = 192;

 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;

 RCC_OscInitStruct.PLL.PLLQ = 7;

 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

 {

Error_Handler();

 }

 /** Initializes the CPU, AHB and APB busses clocks

 */

 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;

 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)

 {

Error_Handler();

 }

}

static void MX_GPIO_Init(void)

{

 GPIO_InitTypeDef GPIO_InitStruct = {0};

 /* GPIO Ports Clock Enable */

 __HAL_RCC_GPIOB_CLK_ENABLE();

 __HAL_RCC_GPIOD_CLK_ENABLE();

 /*Configure GPIO pin Output Level */

 HAL_GPIO_WritePin(GPIOD, LD4_Pin|LD3_Pin|LD5_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pins : LD4_Pin LD3_Pin LD5_Pin */

 GPIO_InitStruct.Pin = GPIO_PIN_13;

 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

 GPIO_InitStruct.Pull = GPIO_PULLUP ;

 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 /*Configure GPIO pin : PD15 */

 GPIO_InitStruct.Pin = GPIO_PIN_15;

 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;

 GPIO_InitStruct.Pull = GPIO_PULLUP ;

 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

}

void Error_Handler(void)

{

}

#ifdef USE_FULL_ASSERT

/**

 * @brief Reports the name of the source file and the source line number

 *   where the assert_param error has occurred.

 * @param file: pointer to the source file name

 * @param line: assert_param error line source number

 * @retval None

 */

void assert_failed(uint8_t *file, uint32_t line)

{

 /* USER CODE BEGIN 6 */

 /* User can add his own implementation to report the file name and line number,

tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */

 /* USER CODE END 6 */

}

#endif /* USE_FULL_ASSERT */

/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

Congrats mate, thnaks for sharing ☺�?​

Hi Bro's,

The weight values ​​are read properly, but how can I calibrate? Do you have any idea about this?

That you will have to solve on your own. Hint: its simple math and known weights.

GSant.3
Associate

Hi everybody... I have the STM32F103C8T6 "bluepill".. i want to conect whit the HX711 using arduino IDE, but doesnt work, someone did this project?

hey i am getting value 1 , 1, 0. like this i am getting !

Please tell what might be the issue !

Thankyou !

hey were you able to solve the 8404695 value issue ?

hi sir i am getting same value when i increased the load also it will not change why i dont know please give me some idea about that0693W00000GW8aoQAD.png