2019-06-05 12:37 PM
The HX711 requires the MCU to send an exact number of clock pulses to capture a 24 bit value, then the clock signal must remain low until the HX711 indicates its ready to transmit again, using the data line. I tried to use a GPIO pin to generate the clock signal manually with pin_set and pin_reset calls, which works in that it creates a clock signal at the frequency of the APB, but the amplitude is only 100 mv. When I plug the clock signal into the HX711 the signal becomes low level noise. Here is the pin config:
/*Configure GPIO pin : SCLK_Pin */
GPIO_InitStruct.Pin = SCLK_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(SCLK_GPIO_Port, &GPIO_InitStruct);
and here is the clock gen code:
// read 24 data bits
for (i = 0; i < 24; i++) {
HAL_GPIO_WritePin (SCLK_GPIO_Port, SCLK_Pin, GPIO_PIN_SET);
buffer <<= 1;
HAL_GPIO_WritePin (SCLK_GPIO_Port, SCLK_Pin, GPIO_PIN_RESET);
buffer += HAL_GPIO_ReadPin (SDATA_GPIO_Port, SDATA_Pin);
}
I should be getting a 3.3V clock signal. Any suggestions?
2020-02-23 10:00 AM
Remember that SCK high longer than 50 us resets the chip. So block interrupts before you set SCK high and unblock after you have reset SCK.
2020-02-24 3:12 AM
HI BROS,
I finally did it.Thank you for your help.
It works properly.
CODE:
#include "main.h"
#include "stm32f4xx_hal.h"
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
uint8_t value=0;
uint8_t i = 0;
int32_t adc_value = 0;
#define pause for(int n=0;n<100;n++){};
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
while (1)
{
while (HAL_GPIO_ReadPin(GPIOD, GPIO_PIN_15));
for(i=0;i<25;i++)
{
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_SET);
//pause
adc_value <<= 1;
if(HAL_GPIO_ReadPin(GPIOD, GPIO_PIN_15))adc_value++;
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_RESET);
//pause
};
for (int i = 0; i < 128; i++) {
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_RESET);
}
//adc_value = adc_value ^ 0x800000;
while(adc_value>=255)adc_value>>=8;
value=adc_value;
adc_value=0;
}
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 192;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 7;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
{
Error_Handler();
}
}
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOD, LD4_Pin|LD3_Pin|LD5_Pin, GPIO_PIN_RESET);
/*Configure GPIO pins : LD4_Pin LD3_Pin LD5_Pin */
GPIO_InitStruct.Pin = GPIO_PIN_13;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP ;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
/*Configure GPIO pin : PD15 */
GPIO_InitStruct.Pin = GPIO_PIN_15;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_PULLUP ;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
}
void Error_Handler(void)
{
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
2020-02-24 4:07 AM
Congrats mate, thnaks for sharing ☺�?
2020-02-25 2:38 AM
Hi Bro's,
The weight values are read properly, but how can I calibrate? Do you have any idea about this?
2020-02-26 12:54 PM
That you will have to solve on your own. Hint: its simple math and known weights.
2020-11-03 1:27 PM
Hi everybody... I have the STM32F103C8T6 "bluepill".. i want to conect whit the HX711 using arduino IDE, but doesnt work, someone did this project?
2021-01-28 3:19 AM
hey i am getting value 1 , 1, 0. like this i am getting !
Please tell what might be the issue !
Thankyou !
2021-02-01 3:43 AM
hey were you able to solve the 8404695 value issue ?
2021-11-01 10:37 PM
hi sir i am getting same value when i increased the load also it will not change why i dont know please give me some idea about that