2020-09-16 04:31 AM
HI All,
I am using STWIN-STWINK1 for a predictive maintenance application, I am unable to set up SWV ITM data console and trace on STM32CubeIDE.
I tried following all the tutorials on YouTube and community, nothing works. If anyone has been able to get this through please let me know or share the configuration.
Many thanks in advance
Chandrashekar C
Solved! Go to Solution.
2020-09-17 07:25 AM
Hi @Chandrashekar C ,
I'm wondering if the SWO pin, required for Serial Wire Viewer (SWV) trace, has been wired on STWINKT1 board... This is an optional pin, as declared by the ST LINK V3 user manual.
The schematic of the application board doesn't seem to include that pin... this may cause the miscommunication.
-Eleon
2020-09-17 06:19 AM
Hi @Chandrashekar C ,
adding more topics for community support.
I find the SWV comsol in Window - Short wiew - other - SWV, and then select for example the SWV Data Trace.
For a tutorial on how to set up the proper variables to be monitored, you can refer to this video.
-Eleon
2020-09-17 06:56 AM
Hi @Eleon BORLINI,
Thanks for your kind response.
I have tried all these and I have also referred to the video you have mentioned in the previous message.
I am trying use SVW console for STWIN_PM_AWS application, instead of terminal, I wan to re-direct all the messages to SVW console.
Here is my debugger configuration
I did changed the puts function as following
/**
* @brief Retargets the C library printf function to the USART.
* @param None
* @retval None
*/
PUTCHAR_PROTOTYPE
{
/* Place your implementation of fputc here */
ITM_SendChar(ch);
return ch;
}
Just wanted to know if I need to enable any macro? or am I doing anything wrong here?
Kind Regards
Chandrashekar C
2020-09-17 07:25 AM
Hi @Chandrashekar C ,
I'm wondering if the SWO pin, required for Serial Wire Viewer (SWV) trace, has been wired on STWINKT1 board... This is an optional pin, as declared by the ST LINK V3 user manual.
The schematic of the application board doesn't seem to include that pin... this may cause the miscommunication.
-Eleon
2020-09-17 07:36 AM
HI @Eleon BORLINI,
This means we can't log printf data to SWV Console on STWINKT1 board?
2020-09-17 07:39 AM
you may use the USART / VCOM interface to implement the printf debug (example)...
-Eleon
2020-09-17 07:58 AM
HI @Eleon BORLINI
I am already doing this, I just wanted to print into SWV console while I am debugging.
Looks like with STWINKT1 its not possbile :-(
Kind Regards
Chandrashekar C