2023-10-18 08:09 PM
I connected the MKI231KA board to the Nucleo-L073 board to test the STHS34PF80.
And I downloaded the PresenceDetection_STHS34PF80 example in the MEMS1 package.
Afterwards, I ran Unicleo-GUI and connected it to the COM port, but the data was not read Normally.
Do I need another setup?
Solved! Go to Solution.
2023-10-20 03:14 AM
Hi @PatrickS ,
I have checked and I replicated your same issue, it's a bug in Unicleo-GUI that will be fixed in the next release. Thank you for notice me that.
In the meantime, you can switch to PresenceDetection_STHS34PF80 firmware and the data should not be zero.
If this solves your problem, please mark my answer as "Best Answer" by clicking on the "Accept as Solution" button, this can be helpful for Community users to find this solution faster.
2023-10-19 03:54 AM
Hi @PatrickS ,
Welcome to ST Community!
Can you share some photos of your setup and screenshots of what you are reading?
Thanks.
2023-10-19 05:05 PM
Hi, @Federica Bossi
I'm sharing screen shot that I tested.
There is no change in user message data whether I connect or disconnect the MKI231KA board.
2023-10-20 03:14 AM
Hi @PatrickS ,
I have checked and I replicated your same issue, it's a bug in Unicleo-GUI that will be fixed in the next release. Thank you for notice me that.
In the meantime, you can switch to PresenceDetection_STHS34PF80 firmware and the data should not be zero.
If this solves your problem, please mark my answer as "Best Answer" by clicking on the "Accept as Solution" button, this can be helpful for Community users to find this solution faster.