Skip to main content
Associate
December 19, 2024
Solved

HDPE triggering Tpresence for STHS34PF80

  • December 19, 2024
  • 2 replies
  • 706 views

We are designing an STHS34PF80 into an occupancy sensor and the plan is to have an HDPE window to protect it.  To test the response in the actual product we purchased 1/16" (1.5mm) HDPE sheet and put it over the sensor.  The fresnel lens with the dev kit was removed.  Surprisingly the Tpresence triggers when the sheet is over the sensor, and so the device doesn't seem to be seeing through the HDPE sheet.

My first thought is that the HDPE is doped or just wrong somehow but I thought I'd ask if anybody else has seen something like this.

Thank you.

This topic has been closed for replies.
Best answer by Federica Bossi

Hi @Megatronic ,

 

When you put the lens in front of the sensor, you are changing the working condition of the system, therefore it's necessary to perform a reset of the algorithm. You can follow the procedure in the AN5867 paragraph 7.4.

2 replies

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
January 3, 2025

Hi @Megatronic ,

 

When you put the lens in front of the sensor, you are changing the working condition of the system, therefore it's necessary to perform a reset of the algorithm. You can follow the procedure in the AN5867 paragraph 7.4.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate
January 8, 2025

Thank you.  That worked.