2021-12-13 11:54 PM
2021-12-22 12:48 AM
Hi @MSchl.3 ,
the issue should now be solved (at least internally)!
It was linked to fast FOTA(not supported by BlueNRG-2- STVELA-IDB008, SensorTile, or BNRG2A1).
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2021-12-15 1:21 AM
Hi @MSchl.3 ,
which hardware platform are you using?
-Eleon
2021-12-15 1:28 AM
Hi, its BlueNRG-232
Markus
2021-12-15 3:19 AM
Ok, I have added more BLE-related topics for more help.
On which ST demo platform is mounted the BlueNRG-232 (e.g. the Sensortile, or else)?
-Eleon
2021-12-15 4:05 AM
I made a small mistake in the title: It is broken since version 4.14 (ST BLE Sensor), it was working in 4.11. !
It is our implementation. We did not change anything. We can select our device in OTA mode within the App, we can select the file in the App at "Select file & flash", but after that the App does not flash anything, we can tap on "Select file & flash" again and again.
It worked perfectly fine in App version 4.11. !
Thanks
2021-12-15 4:54 AM
BTW, it works perfectly fine on the Android version of the ST BLE App ! but not on iOS 4.14!
2021-12-15 7:09 AM
Hi @MSchl.3 ,
ok that's clear, thank you for the update.
But which physical board are you using?
The BlueNRG-232 is just the module that should be mounted somewhere.
And are you using the FOTA taking the firmware file from the smartphone memory?
-Eleon
2021-12-15 7:13 AM
And are you using the FOTA taking the firmware file from the smartphone memory?
Yes
2021-12-15 7:14 AM
Why is it that the OTA update is working on 4.11 (iOS) version, but not on the 4.14 (iOS),
and is working on the Android App ?
2021-12-22 12:48 AM
Hi @MSchl.3 ,
the issue should now be solved (at least internally)!
It was linked to fast FOTA(not supported by BlueNRG-2- STVELA-IDB008, SensorTile, or BNRG2A1).
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon