cancel
Showing results for 
Search instead for 
Did you mean: 

ST BLE Sensor App on iOS is broken since 4.11, does not flash OTA firmware

MSchl.3
Associate II
 
1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Hi @MSchl.3​ ,

the issue should now be solved (at least internally)!

It was linked to fast FOTA(not supported by BlueNRG-2- STVELA-IDB008, SensorTile, or BNRG2A1).

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.

-Eleon

View solution in original post

16 REPLIES 16
Eleon BORLINI
ST Employee

Hi @MSchl.3​ ,

which hardware platform are you using?

-Eleon

MSchl.3
Associate II

Hi, its BlueNRG-232

Markus

Eleon BORLINI
ST Employee

Ok, I have added more BLE-related topics for more help.

On which ST demo platform is mounted the BlueNRG-232 (e.g. the Sensortile, or else)?

-Eleon

MSchl.3
Associate II

I made a small mistake in the title: It is broken since version 4.14 (ST BLE Sensor), it was working in 4.11. !

It is our implementation. We did not change anything. We can select our device in OTA mode within the App, we can select the file in the App at "Select file & flash", but after that the App does not flash anything, we can tap on "Select file & flash" again and again.

It worked perfectly fine in App version 4.11. !

Thanks

MSchl.3
Associate II

BTW, it works perfectly fine on the Android version of the ST BLE App ! but not on iOS 4.14!

Eleon BORLINI
ST Employee

Hi @MSchl.3​ ,

ok that's clear, thank you for the update.

But which physical board are you using?

The BlueNRG-232 is just the module that should be mounted somewhere.

And are you using the FOTA taking the firmware file from the smartphone memory?

-Eleon

MSchl.3
Associate II

And are you using the FOTA taking the firmware file from the smartphone memory?

 Yes

MSchl.3
Associate II

Why is it that the OTA update is working on 4.11 (iOS) version, but not on the 4.14 (iOS),

and is working on the Android App ?

Eleon BORLINI
ST Employee

Hi @MSchl.3​ ,

the issue should now be solved (at least internally)!

It was linked to fast FOTA(not supported by BlueNRG-2- STVELA-IDB008, SensorTile, or BNRG2A1).

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.

-Eleon