2020-10-20 01:54 AM
2020-10-26 11:38 AM
Hi Eleon,
in my last reply I wrote wrongly iBeacons but I mean Beacon with B-L475E-IOT01A
Thank you
Best regards
Luigi
2020-10-27 06:29 AM
Hi @Luigi Bibbo´ ,
well I'm not an expert of the BLE products, and it would be better to ask in the Interface and Connectivity ICs community section.
But not sure that the iBeacon described can run on the B-L475E-IOT01A as-it-is, since it is equipped by the SPBTLE-RF module (Bluetooth 4.1) and not by the BlueNRG-1 or -2 (compliant with Bluetooth v5.0). The example platform is the STEVAL-BCN002V1B sensor node.
In any case, to calculate distance through the RSSI node you need at least two B-L475E-IOT01A devices, and you should implement the calculation by hand...
-Eleon
2020-12-07 10:24 AM
Hi Eleon,
I need ask a question. I wonder if on the B-L475E-IOT01A platform ultrasound / acoustics device can be can be linked to indoor navigation.
Thank you very much
Best Regards
Luigi
2020-12-10 03:39 AM
Hi @Luigi Bibbo´ ,
the B-L475E-IOT01A has a Time-of-Flight and gesture-detection sensor (VL53L0X) onboard, so you might use this device for your application purpose.
-Eleon
2022-06-21 11:14 AM
2022-06-21 11:15 AM
Good morning, I need a reference for the formula of the relative error L2 used for the validation on the desktop and validation on target of the DL model with the generated C model on the host :
where Fj are the outputs relative to the layers of the c model, while fj are those close to the original model.
Thank you very much.
Best regards
Luigi
2022-06-21 11:15 AM