This is the document I am referring to: UM2526 User Manual – Getting started with X-CUBE-AI Expansion Package for Artificial Intelligence (AI), January 2022.
This is link of the board B-L475E-IOT01A - STM32L4 Discovery kit IoT node, low-power wireless, BLE, NFC, SubGHz, Wi-Fi - STMicroelectronicsDISCO-L475VG-IOT01A (B-L475E-IOT01A) | Mbed
Good morning, I need a reference for the formula of the relative error L2 used for the validation on the desktop and validation on target of the DL model with the generated C model on the host :
where Fj are the outputs relative to the layers of th...
Good morning, I need a reference for the formula of the relative error L2 used for the validation on the desktop and validation on target of the DL model with the generated C model on the host : where Fj are the outputs relative to the layers of the ...