2020-05-29 10:11 AM
2021-08-06 02:50 AM
Hello Eleon,
Thanks for the proposal; in fact this was an issue with the TAP_CFG register (a new bit has been created, MSB of this register, which must be set to 1 in order to validate all the interrupts...).
Have a nice day !
2020-06-01 02:22 AM
Hi @TTanm.1 , which kind of failure are you facing? Please note that the two part numbers are slightly different, starting from the WHO_AM_I (0Fh) register: for LSM6DS3 the register value is 69h, while LSM6DS3TR-C is 6Ah (this could turn back into an issue if you are using the Unico-GUI software). Moreover, the mechanical performances are slightly different: are you facing different behavior between the two part numbers on the same application? Regards
2021-07-31 01:39 AM
Hello,
I have also a problem when replacing the LSM6DS3 with the LSM6DS3TR-C : the INT1 pad of the LSM6DS3TR-C is never set to '1', whatever kind of interrupt I configure.
The INT1 pad is configured in push-pull.
Do you have any idea about this problem?
Thank you !
2021-08-06 02:45 AM
HI @odesc ,
did you try setting the INT1 pin in open-drain configuration?
-Eleon
2021-08-06 02:50 AM
Hello Eleon,
Thanks for the proposal; in fact this was an issue with the TAP_CFG register (a new bit has been created, MSB of this register, which must be set to 1 in order to validate all the interrupts...).
Have a nice day !
2021-08-06 02:51 AM
Glad to see you solved your issue!
-Eleon