2017-03-16 9:50 AM
I have a MKI72V1 adapter board. On Unico with V5 it does show up on the devices list however when I select the device I get an error message saying the device is not supported by the motherboard. Please advise.
Solved! Go to Solution.
2017-03-17 3:07 AM
Can you please update the firmware in your board. You need the firmware which is distributed in the STSW-MKI109W together with the Unico v5.0.0.
Please check the directory DFU and the UM0412 - DFU User Guide.pdf for instruction how to update the FW.
2017-03-17 3:07 AM
Can you please update the firmware in your board. You need the firmware which is distributed in the STSW-MKI109W together with the Unico v5.0.0.
Please check the directory DFU and the UM0412 - DFU User Guide.pdf for instruction how to update the FW.
2017-03-17 7:50 AM
Hello and thanks for your response. I checked the DFU folder and it contained the eMotionV5.0.0.dfu file. However After updating FW using this file it still results in the same error.
2017-03-17 8:10 AM
Yes, the eMotionV5.0.0.dfu is the correct file. Are you sure that the FW upgrade was done correctly. Do you see that the firmware version is now 5.0.0 in Unico?
2017-03-17 8:30 AM
Yes it's working now... thank you