cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSO linear acceleration sensitivity tolerance

RBarl.1
Associate

The datasheet for the LSM6DSO does not specify the tolerance of the linear acceleration sensitivity. Can you please tell me what the linear acceleration sensitivity tolerance is for this part.

To be clear, I would expect to find offset and sensitivity accuracy/tolerance figures for linear acceleration and angular velocity:

* LA_TyOff: Linear Acceleration offset accuracy

* LA_So%: Linear Acceleration sensitivity tolerance

* G_TyOff: Angular Velocity offset accuracy

* G_So%: Angular Velocity sensitivity tolerance

The datasheet has three of these (LA_TyOff, G_TyOff and G_So%), but is missing LA_So%.

1 REPLY 1
Eleon BORLINI
ST Employee

Hi @Community member​ ,

from characterization data, I can indicate you +-1% / +-2% as typical value for the LA_So% parameter.

-Eleon