cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6Ds3TR-C embedded temperature sensor accuracy

SSo.1
Associate

I would like to know what the accuracy of the embedded temperature sensor in LSM6DS3TR-C. However, I cannot find this information in the datasheet.

0693W000008xdElQAI.jpg

1 REPLY 1
Eleon BORLINI
ST Employee

Hi @SSo.1​ ,

you are right, but basically all the temperature sensor accuracy is potentially cancelled by the possible temperature offset, that is inside +-15°C at 25°C.

This because the LSM6DS3TR-C is not indeed a temperature sensor, but an IMU equipped with a T sensor.

Suppose however that you have characterized the temperature sensor and you have compensated the offset (and the gain versus temperature, a linear compensation is a good approximation inside the operating temperature range). In this case, stated that the resolution is 1/256°, you can expect something like +-1.5°C accuracy across the +-1°C interval.

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster. 

-Eleon