cancel
Showing results for 
Search instead for 
Did you mean: 

LSM330 SPI register

Hagemu Higuchi
Associate
Posted on March 09, 2018 at 09:34

LSM330 device register is 7bits, but SPI interface express address 6 bits AD5...AD0

Please tell me how to access register higher than 0x40.

1 ACCEPTED SOLUTION

Accepted Solutions
Miroslav BATEK
ST Employee
Posted on March 12, 2018 at 17:56

There is mistake in the datasheet.

Actually the bits in SPI frame used for the address are 7 (MS bit has to be considered as AD6 bit).

We will fix it in the datasheet.

View solution in original post

1 REPLY 1
Miroslav BATEK
ST Employee
Posted on March 12, 2018 at 17:56

There is mistake in the datasheet.

Actually the bits in SPI frame used for the address are 7 (MS bit has to be considered as AD6 bit).

We will fix it in the datasheet.