2020-06-23 7:17 AM
LIS3DE (DocID023719 Rev 3) and LIS3DH (DocID17530 Rev 2) datasheets show the same code ($33) for the WHO_AM_I command? Is this correct? I would expect a different code given one is only 8-bit and the other 8/12-bit.
2020-06-24 7:58 AM
Hi @tonypdmtr , you are right, the only difference between the two part numbers is the fact that LIS3DH is 12 Bit and LIS3DE is only 8 Bit, on the DATAOUT signal. Please note that LIS3DE is now a nrnd product. Regards
2020-06-24 11:47 AM
So, they both respond with $33 from the WHO_AM_I command?
2020-06-25 2:53 AM
Unfortunately yes