cancel
Showing results for 
Search instead for 
Did you mean: 

LIS3DE vs LIS3DH WHO_AM_I command

tonypdmtr
Associate

LIS3DE (DocID023719 Rev 3) and LIS3DH (DocID17530 Rev 2) datasheets show the same code ($33) for the WHO_AM_I command? Is this correct? I would expect a different code given one is only 8-bit and the other 8/12-bit.

3 REPLIES 3
Eleon BORLINI
ST Employee

Hi @tonypdmtr​ , you are right, the only difference between the two part numbers is the fact that LIS3DH is 12 Bit and LIS3DE is only 8 Bit, on the DATAOUT signal. Please note that LIS3DE is now a nrnd product. Regards

So, they both respond with $33 from the WHO_AM_I command?

Unfortunately yes