2023-04-05 10:29 PM - edited 2023-11-20 8:51 AM
Hello,
We are going to use LIS2DE12TR accelerometer, in our ultra low power device, to wake on motion.
Here is schematic for LIS2DE12TR,
Our requirement :
1) ultra low power consumption
2) Wake MCU on Motion by INT_1 Pin
Below are queries regarding schematic:
1) What should be value of R48 and R49.
2) Is schematic is ok?
Thank You
Solved! Go to Solution.
2023-04-07 6:32 AM
Hi @DBhut.1 ,
Yes, the schematic is ok.
The two resistances are not mandatory, you can choose the value you prefer.
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
2023-04-07 6:32 AM
Hi @DBhut.1 ,
Yes, the schematic is ok.
The two resistances are not mandatory, you can choose the value you prefer.
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.