cancel
Showing results for 
Search instead for 
Did you mean: 

Is the pressure port on the lps35hw some sort of a standard? If so, what? Need to know what is available to connect it to vis a vis hose/tubing.

STeag.1
Associate
 
1 REPLY 1
Eleon BORLINI
ST Employee

Hi @STeag.1​ , there isn't a standard "connection" between the pressure port and a pressure tubing, let me say something like a standard pressure fitting. However, hardware guidelines are available for LPS22HB/LPS25HB pressure sensors system integration that can be used also for the LPS35HW. To have something closer to a more standard fitting you could use the LPS33HW, which has a bigger pressure port and is itself water resistant. Regards