2021-02-21 7:48 AM
Hi,
I'm using an ST's digital MEMS microphone in my application. It is connected to an STM32L452 by SPI and the acquired data is stored in an SDCard.
My sampling frequency is 32 KHz which means the microphone produces a considerable amount of data. So, I'm wondering if there is anything that I can do to compress this data within the SDCard.
Any help would be appreciated
2021-02-22 6:03 AM
Hi @Community member ,
I'm not an expert on audio compression techniques on STM32, but as starting point I might suggest you the X-CUBE-AUDIO package that contains a set of audio processing components for the STM32F4 and STM32F7 series (unfortunately not much for L4 family, since usually for audio processing a more powerful MCU would be preferable).
The base is the .wav format, and to reduce the size you could think to:
Let me know if these libraries could be useful for you even if you are using an a STM32L4 MCU.
-Eleon
2021-02-22 7:17 AM
I tend to agree.
Lossy encoding standards like MP3 or OggVorbis require substantial performance.
Surely one can reduce data size per sample, and sampling frequency.
For speech comprehension, even 8kHz is enough.