2019-09-14 9:55 PM
Hi
Is there a way to perform a factory reset for SensorTile? For some reason, my laptop can't detect it anymore. Device manager said "This device cannot start. (Code 10). A device which does not exist was specified." I try to erase full chip flash memory and plan to load the original bootloader, but I also get error message in CubeProgrammer
"Error: Invalid port name: No DFU detEstablishing connection with the device failed"
Pressing the root button doesn't seem to help. I first tried to press the button after connecting to a laptop, but it didn't help. I also tried to hold the root button and release it after connecting to the laptop, but it also didn't help.
May I know what I am missing?
Thanks,
Dennis
2019-10-17 1:02 AM
Please check if you followed these instructions to enter the .dfu mode:
Please check if the ST.box is working via the ST BLE Sensor app. This should work also in case the SD card is not working. If also the .dfu procedure doesn't work, the ST.box is somehow broken.
Regards
2019-10-17 10:11 PM
Hi Eleon,
I am travelling again, but I will give them a try and let you know when I get back.
Thanks,
Dennis
2019-10-19 10:03 PM
Hi Eleon,
One thing I would like to confirm is when I use DFU File Manager, what should be the Target ID and Target Name? Unlike Figure 12 on p.16, there is no Target ID 00, right?
In addition, I am following the steps up to "open the DfuseDemo app and check if your device is recognized". However, the device is not recognized.
I guess the ST.box is somehow broken?
2019-10-30 8:34 AM
Hi @DWang , you should get a screen similar to this one:
Btw, you could do this trial: if your device is detected via BLE by the BLESensor app installed on your device, you can upload the "Data recorder" app. If it's working, then remove the SD card and put it into an external SD card reader, to check the SD card integrity and its content (you should find for example a .csv file containing the data acquired) and to understand if the issue is related to the USB communication. Regards
2019-10-30 9:42 AM
Hi Eleon,
DfuSe Demo didn't detect my device. "Available DFU Devices" didn't list out any device... I still suspect the hardware is somewhat broken...
May I know where to get "Data recorder" app?
2019-10-31 8:08 AM
>> DfuSe Demo didn't detect my device
Ok, so actually I don't exclude the ST.box could be damaged, in this case...
>> May I know where to get "Data recorder" app?
Btw this point works also without the HW working. You open the app and goes to ST BLE Sensor Home --> Create a new App --> Data recorder
Regards
2019-10-31 9:21 PM
I see.
The ST BLESensor app also can't detect my device... I think it is broken now...
2019-11-18 12:22 AM
Dennis, you can ship back to us your ST.box, if you want. We'll repair it and ship back to you for free :) Regards
2019-11-18 9:46 PM
Hi Eleon,
That would be awesome if it can be repaired!
May I know what address I should ship to? Should I address any personnel on the package? And do I need to provide a return envelope?
Thanks,
Dennis
2019-11-21 7:10 AM
Hi Dennis, please check private messages. Regards