cancel
Showing results for 
Search instead for 
Did you mean: 

How to deploy the tensorflow model in the Sensor tile kit.. Is there is any sample code for us to learn and understand how it works

Snara.21
Senior
 
5 REPLIES 5
Imen.D
ST Employee

Hello @Snara.2​ ,

Please have a look at this ST wiki article and video, that may help you.

You can refer to the Getting Started with TensorFlow (via Google search) that shows you how to use step by step the TensorFlow Lite for Microcontrollers.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Snara.21
Senior

Hi @Imen DAHMEN​ 

Thanks for your immediate response. I have followed the instruction shown in "dm00570145-getting-started-with-xcubeai-expansion-package-for-artificial-intelligence-ai-stmicroelectronics" . I have a Tensorflow lite model file, when I try to upload the model. Analyse is working fine, But validation on target . It says StCube32IDE not found

Snara.21
Senior

@Imen DAHMEN​ 

Starting AI validation on target with random data... 

C:/Users/Admin/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/7.0.0/Utilities/windows/stm32ai validate --name network_1627366977421 -m E:/Firmstart/Comtustec/Client_Software/model_int8.tflite --type tflite --compression 1 --verbosity 1 --workspace C:\Users\Admin\AppData\Local\Temp\mxAI_workspace1105783762988500295032472845520054 --output C:\Users\Admin\.stm32cubemx --mode stm32 --desc 115200  

Neural Network Tools for STM32AI v1.5.1 (STM.ai v7.0.0-RC8) 

WARNING: nl_9 (SOFTMAX) in SIGNED not supported. Falling back to float 

Setting validation data... 

 generating random data, size=10, seed=42, range=default 

 I[1]: (10, 30, 32, 1)/int8, min/max=[-128, 127], mean/std=[-1.960, 73.342], scale=0.07154346 zp=17, conv2d_1_input 

 No output/reference samples are provided 

Running the STM AI c-model (AI RUNNER)...(name=network_1627366977421, mode=stm32) 

E200(ValidationError): stm32: Unable to bind the STM AI runtime with "network_1627366977421" c-model: [] 

 connection to "serial:115200"/"115200" run-time fails 

 E801(HwIOError): Invalid firmware - COM4:115200 

I need help to resolve this issue . ia m using Sensortile.box

Imen.D
ST Employee

Hello @Snara.2​ ,

I think this is known issue with X-Cube-AI package.

I will check the status of this issue with the involved people and I'll make sure to post any updates here as soon as they come bak from summer vacation.

I count on your patience and on your kind understanding.

Thanks

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Snara.21
Senior

@Imen DAHMEN​  Hi Any inputs for this issue, this issue comes irrespective of the boards, I validated in STELVAL MKSBOX1V1 and STEVAL - STLK01V1. In MKSBOX1V! the STLINK1 is connected to PA9 and PA10 USART1_RX and TX and I checked the connection using multimeter. Is it possible to support as I need to validate and test a few deliverables