cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I have replaced LSM6DS3 with the LSM6DS3TR-C, but the INT1 pad of the LSM6DS3TR-C is nevers set to '1', whatever kind of interrupt I send. The INT1 pad is configured in push-pull. Is there anybody faced to this problem? Thank you !

odesc
Associate II
 
1 ACCEPTED SOLUTION

Accepted Solutions
odesc
Associate II

Hello,

it works now : there was a bit to set in the TAP-CFG register of the LSM6DS3TR-C, in order to activate all the interrupts (bit which doesn't exist in the LSM6DS3).

anyway, thanks for your help !

Best regards

Olivier

View solution in original post

3 REPLIES 3
TBomb.1
Senior II

Hi, did you tried configuring the interrupt in open-drain? Note that registers can vary a little so that also the configuration code has to be checked.

Tom

odesc
Associate II

Hello,

it works now : there was a bit to set in the TAP-CFG register of the LSM6DS3TR-C, in order to activate all the interrupts (bit which doesn't exist in the LSM6DS3).

anyway, thanks for your help !

Best regards

Olivier

Thank you Oliver for having shared your solution!

-Eleon